Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

SAP and Endress+Hauser work on joint IIoT solutions

Open platform concept for process industry enables seamless integration of field instruments into business processes

Fecha de publicación: 11.06.2018

The goal is to fully integrate the Endress+Hauser field instruments as digital twins into the SAP cloud platform. Both companies want to take advantage of the services and smart apps from SAP’s Leonardo system as well as Endress+Hauser’s IIoT offering.

The idea is to tightly integrate master and sensor data, as well as measurement values, into customer business, logistics and production processes and develop new digital services focused on predictive maintenance and predictive quality. An open platform concept forms the basis for this approach.

“Two innovative companies have come together here to realize the end-to-end OT/IT integration from field instrument all the way to business processes,” said Hala Zeine, SAP’s President of Digital Supply Chain and Manufacturing.

“When it comes to digitalization, successful companies will be those able to tie their systems directly to business processes, thus reliably and fully opening up or circumventing the classic automation pyramid,” explained Matthias Altendorf, CEO of the Endress+Hauser Group. “We and SAP share a common vision of implementing this strategy to the benefit of our customers.”

Endress+Hauser’s role in the partnership involves delivering the field instrumentation knowledge so critical to plant operators in the form of digital services, which will be implemented by integrating the existing Endress+Hauser IIoT services and the SAP platform using a standardized approach.

From the initial creation and automatic updating of a digital twin across the entire product life cycle, to end-to-end connectivity from the sensor to the SAP IT platform, Endress+Hauser is supporting the digitalization strategy of its entire customer base.

SAP demonstrates the concrete benefits of the SAP Leonardo system as an innovation platform. In the SAP Asset Intelligence Network, field instruments are represented as digital twins, which serve as a basis for integration into the customer’s business processes.

Using SAP Leonardo technologies like Machine Learning, Analytics and Blockchain, intelligent services can be flexibly enabled for the production environment. Innovations in the area of maintenance and optimization will help customers achieve the two primary goals of reducing operational costs and increasing productivity.

Descargas

    EH_2018-06-11_Open Plattform Concept.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto

¡Bienvenido a Endress+Hauser!

Seleccione su mercado / región