Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Further growth for Endress+Hauser in China

Third plant inaugurated in Suzhou

Fecha de publicación: 26.01.2018

The opening of the new building, which is situated in Suzhou Industrial Park, a 450-square-kilometer campus that is home to more than 20,000 companies, was celebrated today in the presence of representatives from government and business, as well as customers and employees. The new plant will give the centers of competence for flow measurement engineering, liquid analysis and temperature measurement engineering additional capacity.

“The roughly 44 million euros investment underscores the tremendous significance of the Chinese market,” said Dr Bernd-Josef Schäfer, Managing Director of flow measurement technology specialist Endress+Hauser Flowtec, headquartered in Reinach, Switzerland. The spacious, modern and well-lit production halls and offices provide the ideal conditions for continuing to fulfill the requirements of the Chinese market and the wishes of the customers.

New flowmeter calibration system sets new benchmarks

Apart from an extensive portfolio of measurement instruments, Endress+Hauser also offers a wide range of global services that allow customers to optimize their processes along a plant’s entire life cycle. The result is increased productivity and competitiveness through features such as the fully traceable calibration of measurement instruments.

To date, the Endress+Hauser facility in Suzhou has been capable of calibrating flowmeters with nominal diameters between 2 and 1,200 millimeters. The Group’s largest and most modern calibration facility is now setting new benchmarks.

In the future, the company will be able to calibrate electromagnetic flowmeters in China with a nominal diameter of up to 3,000 millimeters with a maximum measurement uncertainty of ±0.066 percent. That corresponds to a variance of only 100 milliliters for 200 liters of medium – or one champagne glass for a bathtub full of water.

Water and wastewater industries driving growth

Electromagnetic flowmeters with large diameters are commonly used in the water and wastewater industries. One of China’s most important goals is the improvement of water supply across the entire country. Over the last few years, Endress+Hauser has established itself in this growth market through high-quality measurement instruments that reliably and precisely measure the flow of water in treatment plants and distribution stations.

“In order to react quickly and flexibly to regional changes and growth opportunities in local markets, and to stay constantly close to our customers, we are continually expanding production facilities around the world,” explains Matthias Altendorf, CEO of the Endress+Hauser Group, reflecting the Group’s sustainable growth strategy. “This is particularly important in a highly-dynamic market like China.”

Group boasts strong presence in China

Endress+Hauser has been active in China with its own sales center since 1995. Today there are more than 420 sales employees in Shanghai, Beijing and 11 other offices. The flowmeter plant in Suzhou opened in 2004, followed by a second plant for the manufacture of level, pressure and temperature measurement engineering and liquid analysis. Around 290 employees work in production in Suzhou, supplying other countries in the Asian region in addition to the Chinese market.

Laboratory analysis specialist Analytik Jena also maintains a strong presence in China with around 100 employees. The Endress+Hauser subsidiary has operated four locations in the Middle Kingdom since 2001 with a focus on analytical instrumentation and life sciences business.

Descargas

    EH_2018-01-26-Inauguration Suzhou.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto

¡Bienvenido a Endress+Hauser!

Seleccione su mercado / región