Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Leading market position

Frost & Sullivan recognizes Endress+Hauser with the “Global Market Leadership Award” for electromagnetic flowmeters

Fecha de publicación: 07.03.2018

The company was recognized during Frost & Sullivan’s awards gala in California. “Endress+Hauser’s success is tied to a strong customer focus and a high level of innovation,” says Dr. Rajender Thusu, Frost & Sullivan Industry Analyst. The company invests heavily in research and product development in order to meet its customers’ requirements in the area of liquid flow measurements.

Frost & Sullivan highlighted the company’s close collaboration with customers. “Our aim is to help our customers run their processes in a reliable, safe, sustainable and economic manner. To do that, we work closely together with the customers from the very early stages of product design, to the operations phase and beyond,” says Dr. Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec, the Group’s competence center for flow measurement technology in Reinach, Switzerland.

Products and services for individual requirements

The Endress+Hauser product portfolio of electromagnetic flowmeters guarantees precise measurement of volume flow without restricting production flow rates or causing any pressure drop. The result is less downtime and increased productivity, which contributes to lower overall operational costs. “Most of our customers value the combination of state-of-the-art electromagnetic flow measurement instruments and the wide range of services that we offer,” emphasizes Bernd-Josef Schäfer.

Apart from the extensive portfolio of measurement instruments, Endress+Hauser also offers global support services that enable customers to optimize their processes over the plant’s entire life cycle, thus making the company more competitive. This includes calibration, diagnosis, repair, engineering, commissioning and maintenance services.

Leading technologies

The electromagnetic flowmeters from Endress+Hauser, which feature advanced engineering such as Heartbeat Technology, support various communications protocols, including EtherNet/IP and PROFINET, that make the information easily accessible.

Thanks to Heartbeat Technology, instruments such as the Proline flowmeter line have self-monitoring capabilities. By supplying process and instrument diagnostic notifications in line with NE 107, influences and changes can be detected and rectified before impacting the process – all while the process is running.

Descargas

    EH_2018-03_07_Market Leadership Award.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto

¡Bienvenido a Endress+Hauser!

Seleccione su mercado / región