Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Endress+Hauser receives the Red Dot Award

Picomag flowmeter combines outstanding functionality with a solid design

Fecha de publicación: 19.04.2018

The Red Dot is an internationally recognized award for products that feature high-quality design and optimally meet the needs of customers. “We are pleased that the Picomag persuaded the jury with its compact format, flexible installation possibilities and intuitive operation,” said Dr Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec, the Group’s center of competence for flow measurement technology based in Reinach, Switzerland.

Professor Dr Peter Zec, initiator and CEO of the Red Dot Award, congratulated Endress+Hauser: “The winning products are marked by outstanding functionality and an attractive appearance, which proves that the designers understood their customers.” Among other things the products are evaluated according to the level of innovation, functionality, design quality, ergonomics and durability. A roughly 40-person jury selected the winners from 6,300 objects that were submitted for consideration.

Pocket-size flow measurement technology

In industrial process measurement and automation, demand is steadily rising for simple, reliable and maintenance-free measuring instruments in a pocket-sized format. The new Picomag from Endress+Hauser fulfills these requirements and can be deployed across all industries. It measures not only the flow in electrically conductive fluids, but also the process temperature.

In addition, Picomag offers customers easy commissioning with Bluetooth using its SmartBlue App, as well as seamless system integration thanks to IO-Link technology.

Red Dot Design Award

The Red Dot Design Award is one of the world’s biggest design competitions. The award, which stands for outstanding design quality, is divided into three categories: product design, communications design and design concept. Winners will be honored at the beginning of July during the Red Dot Gala, which will be held at the Opera House in Essen, Germany. All of the winning innovations will be displayed during a special four-week exhibition and also presented in the Red Dot Design Yearbook.

Descargas

    EH_2018-04-19_Red Dot Award.zip

Press list

Reciba los próximos comunicados de prensa y noticias directamente en su bandeja de entrada. Asegúrese de estar al día y suscríbase al listado de prensa de Endress+Hauser.

Lista de prensa de Endress+Hauser

Endress+Hauser envía periódicamente comunicados de prensa sobre temas actuales e información de la compañía a los profesionales de los medios de comunicación.

Seleccione los temas que le interesan:  *
Seleccione las industrias que le interesan: *

Datos personales

Los campos marcados con un asterisco (*) son obligatorios. Recibirá un mensaje de correo electrónico con la confirmación de su suscripción. La información proporcionada es voluntaria y sus datos solo se usarán para personalizar los boletines informativos y no se transferirán a terceras partes. Por razones estadísticas, realizaremos un seguimiento anónimo de los enlaces.

Contacto

¡Bienvenido a Endress+Hauser!

Seleccione su mercado / región